Target_Torque

Index.Sub 6071.0H
Data Type

Integer16

  Read/Write
PDO Mappable RX_PDO (1)
Unit  ‰ Nominal_Current

Range

0 to (‰ Max drive current)
Default Value 0
Store Supported No
Description

This object defines the Target torque for Profile Torque mode (tq) and Cyclic Synchronous Torque (cst) (cst) modes. The value is considered proportional to Nominal_Current (Motor rated current). The value is defined as thousandths of the torque, e.g. ‘500’ means ‘50%’ of the Motor rated torque.    

Notes

(1) available with firmware V03r03 or superior.

  • This object is available only with firmware version V03r03 or superior.